Single- and double-row roller bearings in linear motion
Figure 2
Figure 3
Shaft Hardness and Linear Bearing Life
Below is the standard life formula for a rolling element linear bearing, where:
L = Rating life (km)
fH = Hardness factor
fT = Temperature coefficient
fC = Contact coefficient
fW = Load coefficient
C = Basic dynamic load rating (N)
P = Load (N)
L =
(
fH * fT * fC
fW
*
C
P
)
3
* 50
Below are 3 examples of similar type rails with varying hardness measurements. When working through the life calculation formula, we consider only the hardness factor to change, leaving all other factors equal at a value of 1. We can observe the impact that the hardness factor has on bearing performance.
- 420 sst, hardened to Rc40 −> fH = 0.27
L = (0.27)3 x 50 = 0.98 km - 440 sst, hardened to Rc50 −> fH = 0.53
L = (0.53)3 x 50 = 7.44 km - 420 sst, hardened to Rc60 −> fH = 1.0
L = (1.00)3 x 50 = 50 km
Minimize Corrosion and Maximize Life
Figure 4
Cite This Page
Source:
PBC Linear -
“Life Calculation for Linear Guide Roller Bearings”
https://pbclinear.com/blogs/blog/calculating-the-life-of-linear-roller-bearings
Last updated:
November 2025