Linear Motion Systems and Applications Blog - PBC Linear

Steel Linear Shafting

White Paper: Hardened Steel Shafting Comparison

Every linear bearing application requires a linear shaft as the inner raceway. Often it is overlooked, or more often, merely considered insignificant… 

Linear Guide Accuracy

White Paper: Linear Guide Accuracy Eliminates Artifacts

There is a primary need for linear guidance systems that provide consistent repeatable performance. This is especially important in the… 

Linear Motion Product Innovation

Celebrating 40 Years of Linear Motion Product Innovation

This year, PBC Linear marks 40 years of engineering linear motion solutions. One important and well recognized area of success comes from innovation… 

Plain Bearing Linear Guide Slider

What is the 2:1 Ratio for Linear Plain Bearings?

The 2:1 Ratio is a geometric relationship which describes the allowable working space of plain bearings. It is the “Binding Ratio”, which…

Capital Investments Deliver Value to Customers

Capital Investments Deliver Value to Customers

PBC Linear is making substantive investments that reflect their ambitious goal to double the size of the company over the next five years …

Roller Bearing Life Calculation for Linear Systems

Life Calculation for Linear Guide Roller Bearings

Linear motion applications are often found to have not only radial loads but also axial load requirements. For these applications, single…

Difference Between Lead Screws and Ball Screws

Difference Between Lead Screws and Ball Screws

Ball screws and lead screws serve different distinct roles in linear motion systems

Plain Linear Bearing

Simplicity® Plain Linear Bearing Design Factors

Simplicity® linear bearings have 3 application design factors to consider such as size standard, temperature range, load orientation, and running clearances:

Plain Linear Bearings

Simplicity Plain Linear Bearings - Built to Last

See the detailed product features of Simplicity plain linear bearings including more on the proprietary self-lubricating liner that ensures smooth, grease-free operation. Then browse the...

Linear Guide Carriage (cam roller)

PBC Linear Named as Leading Motion Systems Manufacturer by Design World

PBC Linear is a leader in providing quick and customer focused linear motion systems....

Linear Motion Systems for Unattended Retail Kiosks:

White Paper: Linear Motion Systems for Unattended Retail Kiosks

The fast growing acceptance of kiosks and unattended retail purchases has presented new challenges for the design and engineering team…

Linear Actuator Gantry System Design

Design Challenge: Linear Actuators in Gantry Systems

Each day, linear motion design engineers have to be knowledgeable, quick, and agile. That is where the SIMO Series Linear Actuators come in.