Installing Simplicity Sleeve Bearings can be tricky due to the thin aluminum outer shell. Following one of these recommended procedures will ensure proper performance. There...
Simplicity® linear bearings have 3 application design factors to consider such as size standard, temperature range, load orientation, and running clearances:
Linear Bearings from PBC Linear are well suited for washdown environments, sticky substances, weld splatter, extreme temperatures, large particulates, and more.
Light weight shaft and support rail (feather light) are aluminum alloy base materials with a hard coat to which weld splatter, paints, and other contaminants...
At the A3 Business Forum in Orlando, representatives from PBC Linear sat down with Manufacturing Matters to discuss core technologies, new products, and 40 years...
Simplicity® plain linear bearings are designed to withstand most industrial environments, including extreme temperatures, washdown, fine particulate contaminants, vibration…