Linear Motion Systems and Applications Blog - PBC Linear

Linear Guide Carriage (cam roller)

PBC Linear Named as Leading Motion Systems Manufacturer by Design World

PBC Linear is a leader in providing quick and customer focused linear motion systems....

Comparing Lead Screw Motor Connections for Linear Actuators

Comparing Lead Screw Motor Connections for Linear Actuators

There are three basic methods of connecting a lead screw to a hollow shaft motor in order to create an external linear actuator system. Here…

Verticle lead screw linaer actuator load drift

Load Drift in Vertical Lead Screw Linear Actuators

In vertical lead screw actuator applications, lead screw selection is crucial to the safety and success of the system. Prevention of load drift…

Ball Screws

Ball Screws

Miniature ball screw assemblies expand the PBC Linear screw-driven product line.

What is Lead Screw Efficiency?

What is Lead Screw Efficiency?

The efficiency of a lead screw refers to how well a screw converts rotary energy (torque) into linear motion. Lead screw efficiency is…

Linear Screw Actuators

Screw Actuator Product Expansion

Linear actuators, particularly screw-driven actuators, are at the forefront of PBC Linear's expanding product line, designed to meet the growing demand for small and sophisticated...

Lead Screw Straightener

Lead Screw Straightening for CNC and Robotics

The Galdabini lead screw straightener brings automation to production, enhancing precision and increasing output… 

Linear Actuators - Belt-Driven or Lead Screw Driven

Belt Drive or Lead Screw Linear Actuator?

Should one choose belts or lead screws for linear actuator systems… 

Linear Actuators: Factors Affecting Accuracy & Repeatability

Linear Actuators: Factors Affecting Accuracy & Repeatability

The reliable repeatable performance of a linear motion system is the goal of every engineer, but what are the factors that contribute to…

Lead Screw Asssembly

Video - Lead Screw Assemblies Webinar

Video of a webinar on motor and lead screw technologies.

Designing Screw Driven Vertical Linear Slides

Designing Screw Driven Vertical Linear Slides

There are several design considerations to keep in mind when designing vertically situated screw driven linear slides. Keep the following tips…

Miniature Linear Motion Line

Miniature Linear Motion Line

PBC Linear has a large selection of miniature linear motion products from ball-type to self-lubricating guides and a selection of driven…