What is the 2:1 Ratio for Linear Plain Bearings?

2:1 ratio for Linear Closed Bearings

The 2:1 Ratio represents the maximum allowable moment arm distance relative to bearing length without causing binding or motion restriction, ensuring optimal performance in plain linear bearings. PBC Linear introduced this groundbreaking concept for self-lubricating linear bearings many years ago, which is now widely recognized as the industry standard by plain bearing manufacturers. This Binding Ratio defines the geometric relationship between the moment arm distance and bearing length.

Discover your ideal linear motion solution:

Other Related Resources:


Example of the 2:1 Ratio for Plain Linear Bearings

In the image, "2X" represents the distance from the shaft to the load or applied force, while "1X" is the distance between the bearings along the shaft. To maintain the critical 2:1 Ratio, if 2X equals 10 inches, then 1X must be at least 5 inches. Failing to adhere to this ratio can result in binding or restricted movement in the application. 

Troubleshooting Binding in Plain Bearing Applications

There are five simple strategies that can resolve binding or stick-slip problems in most applications. These are listed in no particular order, and the best solution depends on what is most beneficial and feasible for your specific application: 

  • Reduce Moment Arm Distance: This will shift the application out of the binding or stick-slip zone and into the smooth motion zone. 
  • Increase Bearing Length: Options include switching to a longer bearing/carriage, increasing the spacing between multiple bearings, or adding a second bearing to a single bearing system. 
  • Add a Counterbalance: A counterbalance reduces the moment, which in turn lowers the resulting forces and the frictional forces. 
  • Remove External Forces: Misalignment or damage to a shaft/rail is a common source of external forces. Correcting these issues can resolve binding. 
  • Reduce Bearing Friction: Adding lubrication or switching to a different type of lubrication can lower the overall coefficient of friction.

If these strategies don't solve the binding or stick-slip issue, contact a PBC Linear application engineer for additional troubleshooting assistance. 

Troubleshooting Binding in One Direction of Motion

In some applications, smooth motion may occur in one direction but binding in the opposite direction. This is typically caused by previously unaccounted-for forces. While forces are often accounted for along one axis, they are rarely confined to just one. If a force is applied at a distance greater than the Binding Ratio in one axis, the entire system may experience stick-slip motion or even complete binding. This can make troubleshooting frustrating, as the system seems to function correctly only half of the time. The most common solution is to increase the bearing length, either by increasing the distance between bearings or switching to an extended-length bearing. 

‹ ›
Cite This Page

Source: PBC Linear - “What is the 2:1 Ratio for Linear Plain Bearings?”
https://pbclinear.com/blogs/blog/white-paper-demystifying-the-2-1-ratio
Last updated: November 2025