Video: Non-Captive Lead Screw Linear Actuators

Video: Non-Captive Lead Screw Linear Actuators

Non-captive types of lead screw driven linear actuators are different from the more common external versions in that they allow the lead screw to completely pass through the motor. This fundamental difference offers advantages for those that have limited space available or are looking to shrink the overall size of their design package.


With an external actuator, the object being moved is mounted to the nut external to the motor assembly, and the screw rotates providing the motion along the length of the screw.

By contrast, in a non-captive actuator, the screw passes completely through the motor assembly, with the nut housed inside the motor and the payload or moving object attached to the motor itself. As the screw rotates, the motor, load, and nut travel along the screw, while the screw ends are typically fixed to the surrounding equipment.

Because the screw can pass through the motor, this configuration often allows for a longer overall screw length. It is also well suited for external linear guide bearings, which are almost always required in non-captive applications. These guides add stiffness and help prevent deflection, reducing premature wear on the nut, screw, and internal motor bearings.

A less common non-captive arrangement attaches the device or payload to the end of the screw rather than to the motor assembly. In this configuration, the screw translates through the motor as the internal nut rotates. Because the screw itself provides limited stiffness, this approach is suitable only for very light loads and requires external linear guidance to prevent deflection. The design must also provide clearance for the screw to protrude from the opposite side of the motor.

Non-Captive Figure 1
Non-Captive Figure 2

One feature common to all non-captives is that the nut driving the screw is internal to the motor. Traditionally, this nut has been a standard nut with no mechanism to account for the play between the external threads of the screw and the internal threads of the nut. If, in this scenario, an anti-backlash capability was needed, manufacturers might be able to provide a custom solution, but with significantly higher cost and extended lead times.

To avoid this problem, PBC Linear offers the choice of a standard nut or anti-backlash nut within their non-captive linear actuators. We have the only anti-backlash nut and lead screw assembly available off-the-shelf in a non-captive configuration. This unique combination offers the best positional performance available in a non-captive hybrid actuator by utilizing our patented Constant Force Technology (CFT), which provides greater than two-times the superior backlash compensation as tested against competitors.

This advantage means that the self-lubricating nut will provide lubricant-free, consistent performance and preload over its lifetime. In addition, screws are available either uncoated or with a proprietary PTFE coating. These screws come with standard lead accuracy of 0.003 inches per foot, which is three-times better than typical screws on the market.

Non-captive linear actuators from PBC Linear go beyond the simple definition of motor and lead screw. They excel because they have been designed from the inside out, providing superior performance in linear motion applications.

Please be sure to see our full line of Captive and Non-captive lead screws.

›
Cite This Page

Source: PBC Linear - “Video: Non-Captive Lead Screw Linear Actuators”
https://pbclinear.com/blogs/blog/non-captive-linear-actuators
Last updated: November 2025