Lead Screw applications for medical devices and laboratory automation
As medical diagnostics, devices, and laboratories have become more reliant on automation and laboratory processing, a need has grown for more refined and dynamic linear motion systems. PBC Linear has emerged as a leader in advanced lead screw systems, providing higher quality screws with tighter tolerances, and a better overall product solution to the standard belt drives. Depending on the application, our lead screws can provide an appropriate combination of accuracy, positional repeatability, and consistent linear motion speeds that meet application requirements, and ultimately help to balance cost with overall effectiveness.
First, it is important to understand the type of application that you’re going to build on. We break these down into three main categories within the medical genre: precision, transport, and set-up applications. Each of these application categories, as further explained below, has its own unique requirements to operate successfully in medical environments. The value to OEMs, medical institutions, and ultimately patients depends on how lead screw systems are selected, implemented, and eventually how they can dramatically improve the overall equipment effectiveness (OEE) within these medical devices and automated systems.