What do the terms accuracy and repeatability mean?
- Accuracy refers to the ability to achieve a commanded position
- Repeatability refers to the ability to go to any given spot in a consistent grouping
Does PBC Linear offer ball bearings that are corrosion resistant?
Does the EPK25G flange mount have seals?
Does the IPP series of pillow blocks have seals?
Is the IP-G series of linear ball bearings self-aligning?
What is the temperature range for linear ball bearings?
Are the rollers replaceable on the IVT carriages?
Are the rollers replaceable on the Redi-Rail sliders?
Can Hevi-Rail be welded?
Yes. Bearings with pre-welded flange plates are only capable of the system max. Static load capacities shown in the CRT (Cam Roller Technology) catalog. The actual bearings are rated for higher load ratings if configured without the pre-welded flange plate and utilized with customer supplied Hardened Rail HRC 55 (minimum 2.54 mm depth provided).
Is it correct that the version of the Hevi-Rail bearing without the welded flange plate, has a higher load capacity than the version with the welded flange plate?
Yes, that is correct. The Welded Bearing/Flange Plate Assembly is rated to accomodate up to the System Maximum Static Load Ratings as published in the CRT (Cam Roller Technology) catalog. These same "System Maximum Static Load Ratings” also apply to the maximum load rating that the Mild Steel U-Channels and I-Channels can accommodate on a per. Roller basis. These are the limiting factors in the system.
Can you replace just the rollers on a Redi-Rail slider?
Does PBC Linear offer heat treated versions of Hevi-Rail channels?
A word of caution: If you’re considering outsourcing Heat Treatment of Hevi-Rail Channels, discuss, review and potentially test samples with a Heat Treatment Specialist for best methods of Heat Treatment. Improper Heat Treatment methods may result in material distortion, bowing and stress fracturing of Hevi-Rail Channel.
The S450J2 MOD. material can be heat treated, but usually requires a re-straightening after heat treatment due to warping from the heat treatment if the whole bar is heat treated.
Preferred Method - Surface hardening with induction heating with a mechanical clamping or guiding of the bar through the induction coils is what others use that prevents warping.
Improper Heat Treatment of Hevi-Rail channels can lead to bowing - twist distortion and stress fracturing of channel.
Does PBC Linear provide wrenches for the Commercial Rail and why would I need one?
Does Redi-Rail have a reference surface to aid in rail alignment?

How can I tell the difference between compensated and precision Mini-Rail carriages?
How do I protect Hevi-Rail products from oxidation and corrosion?
PBC Linear suggests sand blasting or bead blasting Hevi-Rail channels to remove any signs of oxidation or rust that may have been acquired during shipment and storage. Then follow-up with one of the following coating suggestions:
- PBC Linear suggests priming, painting and / or powder coating the Hevi-Rail Channels. Surfaces on the Hevi-Rail Channel surfaces that are considered Roller Contact surfaces, should be masked prior to applying the coating. Roller contact surfaces must remain bare steel surfaces, but coated with NLGI #2 or Grade 3 Grease to minimize oxidation and corrosion.
- A Hard Chrome Plating or Armoloy (TDC) Thin Dense Chrome Plating can be applied by the customers plating resource to the Hevi-Rail Channels for oxidation and corrosion resistance. An NLGI #2 or Grade 3 Grease should still be applied to the Rollers and Roller contact surfaces of the Rail to increase life expectancy.
How do you mount Hevi-Rail bearings?
How do you mount the PAC2247?
Is Hevi-Rail available in stainless steel?
Is IVT available with stainless steel rollers and raceways?
Is the load rating for Redi-Rail sliders per slider or per pair?
Is V-Guide rail hardened?
We have Redi Rail sliders with a threaded stud shaft, and we recently ordered some more. The ones we received don’t have replaceable rollers. We’d really like the same style as the ones we already had, are they still available?
What are the Hevi-Rail mounting plate holes intended for?

What do the arrows on the Redi-Rail slider mean?
What is the average C.O.F. range for a IVT Carriage?
What is the average cof of the LPM slider/rail system?
What is the operating temperature for Hevi-Rail?
What is the operating temperature for Mini-Rail?
What sizes of Simplicity bearings have the seal option?
What is the operating temperature for Redi-Rail?
What is the operating temperature for the Hardened Crown Roller series?
What is the operating temperature for the low profile Mini-Rail?
What is the operating temperature for V-Rail?
What is the operating temperature for Integral-V Technology?
What kind of lubrication should be used on Hevi-Rail?
What kind of screws are needed for Redi-Rail?
What size T-Nuts fit the Uni-Guide?
Why does the CRT (Cam Roller Technology) catalog identify Hevi-Rail with multiple Load Ratings for each size product?
Each Size Hevi-Rail product is specified with System Max. Static Load Ratings per. Roller for both Radial & Axial Load Capacities which shouldn’t be exceeded when using the Mild Steel U & I Channels that PBC Linear offers. This System Max. Static Load Rating takes into account operating the Roller on a soft Mild Steel Rail.
Each Size Hevi-Rail Product is also specified with Maximum Bearing Loads (Static and Dynamic) per. Roller which requires the usage of Heat Treated Channels that PBC Linear doesn’t offer. Note: Maximum Bearing Loads achievable when used with a hardened rail HRC 55 minimum 2.54mm deep.
Why is the load rating of the bearing much greater than the load rating of the system?
Why is there a discrepancy between the height of the V-Guide Rail in your catalog and the actual height of the V-Guide?
Are PBC Linear products REACH compliant?
Are PBC Linear products RoHS compliant?
Does PBC Linear offer a curved track?
How do I receive the CAD file for my part number?
I am interested in the corrosion resistance of your aluminum components and slides.
For more information please see our Linear Motion Design in Washdown white paper.