Will MTB belt-driven linear actuators back drive?
Yes, MTB actuators can back drive in certain circumstances unless their drive train is designed to prevent it. MTB actuators are highly efficient, utilizing belts and pulleys to drive the carriage and linear guides with ball bearings to maintain linear motion. For example, in a vertical application with a weight load on the MTB carriage, the carriage may drop if power is removed from the drive motor unless a brake or other device is installed.
Can MTB belt-driven linear actuators be used in vertical applications?
Yes, MTB actuators can be used in vertical applications. A brake on the drive motor or other device may be required to prevent a weight load from dropping if power is removed from the drive motor.
Are motor mounts available for the MTB linear actuators?
Yes, motor mounts are available for MTB actuators. Contact PBC Linear application engineers for more details.
Can users request which side the male drive shaft sticks out of an MTB actuator?
Yes, users can specify the side for the male drive shaft or request a male drive shaft on both sides of the actuator.
Can users request a hollow drive shaft for an MTB linear actuator?
Yes, the MTB042, MTB055, MTB080, and MTB105 models can be ordered with hollow drive shafts.
What are the drive shaft diameter options for MTB linear actuators?
| Actuator Model | Male Shaft Diameter | Hollow Shaft Diameter |
|---|---|---|
| MTB042 | 12 mm | 10 mm |
| MTB055 | 16 mm | 12 mm, 14 mm |
| MTB080 | 19 mm | 16 mm, 19 mm |
| MTB105 | 25 mm | 22 mm, 25 mm |
What is the maximum body length of an MTB042 actuator?
| Actuator Model | Maximum Length | Consult for Lengths > 1,500 mm |
|---|---|---|
| MTB042 | 2,000 mm | Yes |
| MTB055 | 6,000 mm | Yes |
| MTB080 | 6,000 mm | Yes |
| MTB105 | 6,000 mm | Yes |
What is the maximum body length of MTB055, MTB080, and MTB105 actuators?
The maximum length is 6000 mm. For lengths exceeding 1500 mm, consult PBC Linear engineers.
Can MTB linear actuators have more than one carriage?
Yes, MTB actuators can be supplied with multiple carriages, all moving in the same direction. The number of carriages and their spacing must be specified at the time of order. Opposing movements in the same actuator are not possible.
Can multi-axes systems be made using MTB linear actuators?
Yes, multi-axes systems can be created by mounting the body of one MTB actuator to the carriage(s) of another. Contact PBC Linear engineers for information on mounting plates.
Do MTB linear actuators require lubrication or maintenance?
Inside the MTB actuators, there is a linear guide rail and bearing blocks to guide the actuator’s carriage. Lubrication should periodically be applied to the linear guide rails to keep the ball bearings and raceways lubricated. The frequency of lubrication will depend on the duty cycle, speed, and load. The guide rails can be accessed by removing the holders of the seal strips at the end of the actuator and moving the seal strip. The belt can be flexed out of the way to allow grease to be applied to the rail beneath it.
Can sensors be installed on MTB linear actuators to detect carriage position?
Yes, sensors can be installed in the t-slots on the sides of the MTB actuators to sense carriage positions. Mounting brackets for barrel-style proximity sensors can also be mounted to the t-slots. Contact PBC Linear engineers for more details and part numbers.
Can users request or install connections for pressurized air to MTB actuators as an added barrier to prevent the ingress of dust and debris?
Yes, users can request or install connections for pressurized air. However, the air pressure and flow rate must be controlled carefully. Excess pressure or flow will cause the seal strip to rise off the magnets that hold it to the actuator body.
What material is the seal strip made of on the MTB and PLA linear actuators?
A 400 series stainless steel is used to ensure compatibility with the magnetic strips along the opening.
What T-nuts are used for MTB linear actuators?
| Actuator Model | Nut Type | Part Number |
|---|---|---|
| MTB042 | Low-profile nut (M5 screws) | 6100504 |
| MTB055 / MTC042 | Short T-nut | 6100443 |
| MTB055 / MTC042 | Long T-nut | 6100429 |
| MTB080 | Slot size 6 T-nut | 6100435 |
| MTB080 | Slot size 8 T-nut | 6100436 |
Are the drive shafts timed with the pulleys when driving two linear actuators in parallel?
Currently, the female (hollow) shaft version is not timed between the hollow shaft and the pulley. However, the male shaft version maintains timing because the internal and external keyways are manufactured simultaneously. In the future, the female shaft version will also be manufactured with timed keyways.