Linear Motion Systems and Applications Blog - PBC Linear®

Sleeve Bearings

Simplicity Sleeve and Flange Bearing Installation

Installing Simplicity Sleeve and Flange Bearings can be tricky due to the thin aluminum outer shell. Following one of these recommended procedures will ensure proper...

Linear Bearings: Plain vs Ball Bearing?

Plain Linear Bearings vs Ball Bearings in Washdown

Simplicity linear plain bearings will not catastrophically fail when exposed to frequent washdown cycles. Additionally, Simplicity's Frelon liner…

What is the 2:1 Ratio For Linear Plain Bearings?

What is the 2:1 Ratio For Linear Plain Bearings?

The 2:1 Ratio is a geometric relationship which describes the allowable working space of plain bearings. It is the “Binding Ratio”, which…

Design Factors for Simplicity Bearings

Design Factors for Simplicity Bearings

When designing applications to use Simplicity linear bearings, there are factors to consider within your application such as size, temperature… 

Leaders in Innovation

Leaders in Innovation

PBC Linear is a leader in providing quick and customer focused solutions to the toughest linear motion problems by making substantial time…

White Paper: Linear Motion for Fitness Equipment

White Paper: Linear Motion for Fitness Equipment

As the field of specialized fitness equipment has grown, so has a proliferation of various designs and configurations for both the equipment and…

Bearing Solutions for Harsh Environments

Bearing Solutions for Harsh Environments

Its time to hang up the gloves and combat environmental issues with a PBC linear motion guidance solution. What are the best practices for… 

Cantilevered Loads and the 2:1 Ratio

Cantilevered Loads and the 2:1 Ratio

One of the most frequently misunderstood principles regarding the use of plane bearings is the 2:1 Ratio. This is the allowable moment arm…

Non-Standard Housings and Self-Alignment

Non-Standard Housings and Self-Alignment

Not all linear motion applications are the same. That is why Simplicity self-lubricating bearings are offered in a range of options designed…

Linear Shafting and Rails Light Weight Alternatives

Linear Shafting and Rails Light Weight Alternatives

Light weight shaft and rail (feather light) are aluminum alloy base materials with a hard coat to which weld splatter, paints, and other contaminants will…

Linear Motion Technology Forum Discussion

New Linear Motion Technologies at PBC Linear after 42 Years of Innovation

At the A3 Business Forum in Orlando, representatives from PBC Linear sat down with Manufacturing Matters to discuss core technologies, new products, and 40 years...

Simplicity Linear Bearings More Economical

Simplicity Linear Bearings More Economical

Designed to withstand most industrial environments, including extreme temperatures, washdown, fine particulate contaminants, vibration…