Motion Control of Lead Screw Linear Actuators - Webinar
📄 View Video Transcript
0:00
today's webinar integrated approach to motor and lead smooth technology now I'd
0:05
like to introduce our presenters Jamie Stockton is global product manager for PBC linear he has been in the industrial
0:13
automation market for a decade offering engineering support for both mechanical and electrical solutions he has deep
0:20
background in diverse applications including packaging medical aerospace defense and various food-grade
0:27
situations and applications and the score nkow is the Sales Director from
0:33
lunes industry of america inc and he has worked in the industrial automation market for more than 14 years focusing
0:40
on electromechanical products and working with customers on applications across many industries his goal is to
0:46
bring value to his customers to his engineering and customer service background and finally mike maloney is
0:53
the application engineering manager at applied motion products previously he worked as a design engineer at AMC where
1:00
he contributed to the design of several motor drives and played a central role in the development of can open
1:06
compatible drives and integrated motors more recently he has worked in the medical and industrial device market and
1:13
now I'm going to turn the presentation over to the speakers all right thank you
1:18
very much hi this is Jamie Stockton thanks for joining us today what we're going to do
1:24
is go over PBC's integrated approach to motor and leadscrew technology first of
Agenda
1:30
all on the agenda we're going to go over the foundational elements of load leadscrew motor including the control
1:37
motor screw and the nut and then we're going to go through some of the applications that are typically seen for
1:45
this type of product and kind of explain how using the PBC solution it's going to
1:52
help optimize and make those solutions as good as possible first up let's go over what a traditional mechatronics
1:59
based solution looks like you're going to have the screw and nut of course there's two different types of screws
2:06
involved you've got a lead screw which is going to be typically a metal or
2:11
plastic on the screw or you may have a ball screw which
2:16
is essentially rolling-element balls traveling on the screw typically those are going to be the two types of screws
2:23
that you're going to see you're going to have interface Hardware this screw must connect to the motor in a traditional
2:29
system you'll have a coupling and if you have the motor to the system you're going to need some type of motor adapter
2:36
say like a NEMA 17 or NEMA 23 adapter let Annie talk about the different types
2:41
of motors that you might see there's many types of motors obviously the moon's manufactures and with an
2:46
integrated product we could look at a traditional stepper NEMA 1723 or any variety of both depending on your loads
2:52
and torque requirements as well as a step servo product with my chrome Cheryl highlight from ANP which brings the
2:58
technology closer to a servo type performance but with a stepper type commercial side by the motion products
3:06
part of this picture is that we make motor drivers and integrated step motors using the moon's step motors we have
3:12
both open and closed loop drivers including the step server technology that's that's shown there and that
3:18
effectively puts a closed-loop motion controller on the back of the stepper motor which enables like Andy was saying the servo style performance in this
3:25
cost-effective integrated package and we'll talk about that a little bit later moving on to the controller side of
3:32
things in the traditional arrangement here the motor drive physically sits between the controller and the motor
3:38
screw combination on the bottom there we have a standard motor drive an P drives
3:43
all have built-in i/o and come in a wide variety of control options from step and Direction locally stored programs to a
3:49
full range field bus control options this motor drive on the bottom is effectively identical to the one on the
3:56
back of the step server smart motor next to it meaning you have a choice of where you want to put the drive electronics
4:01
either directly on the line attached to the motor or back in your control panel where you cable out to your motor and
4:07
then on the top there we see a PLC for many traditional applications a full-time controller like that PLC is in
4:14
the mix either two coordinated motion across multiple axes or even just to monitor the status and a little more
4:19
detail than using the drive digital outputs as I mentioned before our drive support a wide variety of these PLC
4:25
control options from step into affection to various field buses really the drives can interact with pretty much
4:31
any PLC you throw at it to enable control of this traditional motor lead screw system alright that was what a
Optimized System Overview
4:38
traditional setup would look like and now this picture will kind of go over what the optimized PBC offering is going
4:45
to entail we've got the lead screw and the lead screw nut as you can see and
4:52
we'll talk about a little bit more later the coupling and motor mount adapter are not present as we've directly coupled
5:00
the screw to the motor we've got the moon's stepper motor which is a hollow
5:07
shaft as you can see from the picture below Andy maybe you could talk about that picture just a little bit what you
5:13
see is a cutout of the motor and with this integrated solution or optimized system we've got a hollow bore offering
5:20
that we'll talk about a few of the benefits of the hollow bore with with our partnership PBC essentially
5:26
integrates that screw into the motor and allows for again a tighter package we eliminate some of the mechanical
5:31
components that couple the screw it allows for a number of advantages and
5:36
efficiencies on the customer side bigger bearings for your axial loads that are translated etc but we will touch on that
5:43
a little bit more when we get into the details of the motor and if you can read the chart on the bottom left very well
5:50
then you have better eyes than I do but perhaps my can elaborate a bit on what that means and what the back of the
5:57
motor has on it there that picture is just a generic closed-loop control system on the control side we have the
6:03
same basic drive interface that we had in a traditional system but here again it's closely coupled to the motor and
6:09
the screw for a tight integrated package you get all the same local real control options as in the traditional system but
6:15
here again they're optimized out-of-the-box for the specific motor and leave screw combinations to really produce the integration time now we're
Constant Force Nut Overview
6:22
going to talk a little bit about the nut to nut that PBC is offering which we
6:29
actually just released as a general product release a couple of weeks back is a patented anti backlash design if
6:36
you look at the two pictures on the right hand side the one on the top is the PBC nut we're calling this nut a
6:44
constant force anti backlash nut and you can see it looks quite a bit different than the traditional anti backlash
6:52
spring nut what we have found through great amounts of testing is that we are
6:58
offering better than two times anti backlash compensation using the constant
7:04
force anti backlash nuts this also offers a more consistent
7:09
preload over the life of the system to elaborate that a bit more typically when
7:16
you use a spring loaded anti backlash nut as the nut wears in the amount of
7:21
preload varies and it actually varies quite a bit what that normally means is
7:26
that when you have an application you run it for some period of time until you see that backlash start to wear in and
7:34
then you have to go into your system and do some adjustments to compensate for that backlash change the constant force
7:42
technology essentially eliminates the need for that step as the backlash stays
7:47
very consistent over the entire life of the nut also worth noting the PBC line
7:54
which we are offering an anti backlash nut as you see here and a standard nut
8:00
which is no anti backlash they're both going to be made as standard from a self
8:06
lubricated PTFE type of Delrin and with that we would recommend using no
8:12
lubrication in the system where with the traditional nut made of acetal or other
8:17
types of plastic traditionally lubrication is going to be recommended we're saying this is two to four times
8:24
better than traditional designs in terms of backlash and wear the next slide is a
8:31
45 second video which will go over a comparison of these two nuts
8:37
side-by-side PBC is proud to introduce a full line of lead screw products
Constant Force Overview
8:42
featuring an anti backlash technology and we call constant force the visual difference is evident let's take a
8:49
closer look the conventional design has a variable and inconsistent radio force which changes
8:55
dramatically over the life of the application the traditional product uses a spring while the constant force uses a
9:01
band the constant force band applies uniform pressure to the three fingers which means the preload is consistent
9:08
most importantly testing has shown that our technology maintains preload better over the life of the application
9:18
[Music]
Screw Manufacturing Process
9:24
all right on to the next slide we're going to talk about the actual manufacturing of the screw process which
9:31
is done at PBC here in Illinois we have come up with a unique roll threading
9:36
process and this unique roll threading process will help reduce the amount of
9:41
pitting and flanks compared to a traditional lead screw if you look on the pictures on the right-hand side
9:47
you'll see the PBC screw at the top is very smooth where the screw at the
9:53
bottom is much more rough and jagged essentially what we found through lots
9:59
of life testing is that the smoother screw helps reduce the wear on the plastic nut which was able to allow us
10:07
to get in excess of 6,000 linear miles in a system without failure we also have
10:14
a medical customer that had done some life testing and came up with very
10:19
similar results and of course we'll put the asterisk in there and say depending
10:25
on the application he may or may not see 6000 miles but we were very pleased with
10:30
the results that we found in comparing traditional screw to the screw that PBC
10:35
has come up with in our proprietary manufacturing process also note on here
10:41
and it kind of talked about it at the end of the video we do have an online configurator already set up that will
10:49
allow you to configure 8 the screw nut or lead screw motor in its entirety and
10:54
give you this pricing CAD models pretty much everything that you would expect and doing design type of work to talk
Screw Accuracy
11:01
about accuracy a little bit the screw that we are offering at PBC has about
11:07
two to three times better lead accuracy than a standard industry brew we're at
11:13
plus or minus three thousandths per linear foot traditionally it really depends on the actual manufacturer but
11:19
some of them go as high as 10,000 per linear foot it's definitely better than a traditional screw we've also got
11:27
sophisticated process for testing the screws to ensure that we're actually achieving the accuracy that we are
11:33
stating as you can see on the right hand side we're measure during every single screw that comes off
11:39
of the line over the entire length and we do offer as a special a precision
11:45
screw that's 1000 plus or minus one thousandths over the course of each foot
11:50
and lastly I want to talk a little bit about the motor and screw integration
Motor Screw Integration
11:55
which was sort of alluded to at the beginning here but essentially the top
12:01
picture shows you the motor coupling and screw and the bottom picture shows you
12:08
the PBC solution which has this screw directly connected to the motor via
12:14
laser welding benefits of this is that you've got factory alignment with the
12:21
PBC solution so it's coming to you guaranteed to be very well aligned
12:26
you're going to have fewer components which is going to give you higher rigidity and of course with your
12:33
components you're going to have more reliability and you're going to save money on couplings and other components
12:40
if I could add one other thing with regards to the integration of the previous slide you're actually saving
12:45
space as well so an customer the OEM gets the benefit from either additional
12:51
travel in the same package or they would be able to reduce the size of their package which obviously helps in
12:57
tabletop solutions real estate is always a premium regardless of where your
13:03
machines are going that is an added benefit to squeeze out that extra travel or extra space looking at the motor
13:09
specifically moons as manufacturing over 10 million hybrid steppers a year and growing and we're constantly innovating
13:17
and looking at the technology to see where we can squeeze more out of every single motor leads manufacture whether
13:23
it's our standard or looking at special technology I'll highlight a few of them a couple of them are specific to the
13:30
integrated package but we're also looking at the entire motor technology and capability of moons here just to
13:35
highlight some of the benefits of working with a partner that specializes in motor technology we do have products
13:41
that are available with 30% more torque in the same package we are able to do
13:47
this by adding additional magnets into the rotor and backing into the stator and allowing the direction of the flux to
13:54
increase the amount of torque output this leads to better acceleration and deceleration performance which
14:00
inevitably leads to better cycle times just improve the efficiency on the customer side as well as again the space
14:07
savings in terms of the motor package itself for the amount of torque that you can get out of it interesting technology
14:13
to apply to specific applications for the hollow bore motors we add larger
Hollow Bore Motors
14:19
bearings into the motors themselves because of the additional thrust coming
14:24
from the screw and a linear translation it allows for better support in the axial direction which allows for longer
14:31
life we want to keep up with the 6,000 miles I'll say of linear translation from the PBC screws we need to make sure
14:38
that our motors can withstand that type of travel and life as well and we do that by adding larger bearings in order
14:45
to withstand that load the hollow shaft concentricity doesn't Jamie mentioned factory established type of quality
14:52
coming right out of the line we make sure that the concentricity is tight on the hollow bore which allows PBC to join
14:59
the shaft onto the motor without having any sort of issues in terms of run-out this again inevitably leads to longer
15:06
life smoother operation quieter operation you're getting a quality product straight out of the factory we
Wave Washer
15:13
add a preload to the bearings to eliminate axial play so a standard rotary motor will typically have a wave
15:19
washer installed on one of the sides of the motor so either the front or the rear what this does is it allows for a
15:25
bit of plane give in a traditional rotary application which is good because it extends the life of the bearing but
15:31
for a linear application where you're positioning is critical that's kind of the whole point here you can't have
15:38
essentially 0.9 millimetres of place sometimes with the traditional NEMA 17 it eliminates all of the accuracy the
15:44
precision that is required in a lot of these applications we apply preloaded up
15:49
to eliminate that plate and allow for very good positioning a linear
15:54
applications and then in terms of encoders feedback etc quite often when
16:01
you're relying on that precision accuracy you need the feed do I ensure you're moving ensure you're
16:06
in position and it's standard for us to apply a rear shaft as well as have encoder holes on the back of the motors
16:12
that's easily done and a variety of feedback options available from us again
16:18
depending on the application requirements extremely flexible manufacturing very customized for OEMs
16:24
very flexible and top of the line in terms of technology and always pushing
16:29
furthers we work with customers quite a lot in understanding their applications and using our education along the way in
16:37
order to provide them with the best solution just a quick comment on that
16:43
encoder mounting provisioning the motor lines that we're offering for our leadscrew motors are NEMA 8 through NEMA
16:50
23 and the moons motors that Andy is talking about all have the two holes as
16:57
standard in the back of the motor or for that encoder mounting and since it's a
17:04
hollow shaft motor you'd need to get an option to wear the lead screw would actually stick out the back so that you
17:11
can mount that encoder on there and get the encoder feedback if that's something that your application requires the only
17:17
one that doesn't have the holes would be the aneema eight I don't think they've got poles in that one but the other ones
17:23
all definitely do have encoder mounting capability if we move on to a little bit
Special Capabilities
17:30
more detail on the special capabilities of moons a few of the things I'd like to
17:36
highlight there's a number of ways to address each one some of them I'll highlight here in regards to velocity
17:43
smoothness and scanning Jamie mentioned that all of the meat screws from PBC are
17:49
tested for their precision and linear accuracy and in terms of scanning
17:54
applications absolutely required to have the smoothness not only on the screw but as well as the motion we do have 0.9
18:00
degrees step angles available a traditional step motor is 1.8 degrees so giving you 200 full steps per revolution
18:07
the point nine degrees stepper cuts that in half and allows for 400 full steps and again with micro stepping technology
18:14
which mic might hit on you're able to make those it's even smaller we minimize the torque
18:20
ripple through a variety of ways but one of the main ones is to offer a three-phase stepper which minimizes that
18:27
torque ripple we can talk about that more offline if anyone has any questions high speed motors so we do have stub
18:33
motors that do actually get up to 8,000 rpm if not 20,000 in certain special
18:38
applications this allows for us to get into a higher torque reign the slower
18:44
you go the more torque you have with a step or just to simplify things by allowing a step angle to increase we
18:50
reduce the resolution however we push the amount of torque that you can get to higher speeds again application
18:56
dependent what your requirements are for your linear speed and force we're able
19:01
to adjust either the type of motor we're providing to you guys or able to adjust
19:08
the linings themselves depending on what the application requires and the power you have available to input together
19:14
with a high lead screw either a 25 millimeter per rev range per Rev we have been able to achieve over 1 meter per
19:21
second with a traditional stepper and a high lead lead screw the speed range
19:26
gets quite nice and the flexibility is there to address any application challenging environments temperature
19:32
extremes who get up to class F classification on the motors themselves we've done higher temperature designs
19:37
really comes down to the windings the cables the bearing life we address those
19:43
on an everyday basis IP 65 67 beyond will highlight an anti-corrosion
19:48
technology that we also have available we have seen a number of applications we take that knowledge and it's available
19:54
to our customers in order to benefit from that and get a shortcut in their design process and then customized
20:00
cabling and wire harnesses our company has a division for 600 people strong that focus strictly on wire harnesses
20:07
and that allows us to pass that benefit and optimization on to our end user
20:13
whether it's cables or connectors or shaft modifications but in this case PTC does a great job of that with the Linney
20:18
lead screws you can get those customizations and configure those as needed Mike tell yours yeah thanks Annie I'm
StepServer Technology Advantages
20:26
going to talk a little bit about the step server technology advantages that we mentioned earlier and then a bit about your control
20:32
options to make these systems actually move on the right there you see one of amps step server integrated motors this
20:39
has a moons motor on the front and a full closed-loop control system with a 20,000 line incremental encoder on the
20:46
back but one of the biggest advantages of the steps or technology over a standard stepper motor system is that
20:52
closed loop servo file performance if you think about a classic stepper motor
20:57
drive it has a motor current setting and the motor drive always delivers that set current into the motor regardless of the
21:03
actual load this means that you to set your drive to deliver the maximum required at any point in your move even
21:09
when your motor doesn't need it so as an example if you need five amps to do a quick accel during a long move the drive
21:16
will deliver five amps during the Axelle also five amps during the move and also five answering the D cell to ensure that
21:22
you won't stall and lose position this means that during the long move in the D cell you're potentially burning energy
21:29
you don't need and you pay for that in motor heating and energy costs by contrast this step server technology
21:35
only delivers the current it needs to move the motor as requested in that same example above will set the motor current
21:41
to five amps maximum the motor will accelerate into the move and use the full five amps but once that
21:46
acceleration is complete the torque requirements drop and so the current backs off to the minimum required to
21:52
maintain the desired move profile using that twenty thousand line encoder for reference so this automatically lowers
21:58
the current consumption of the motor which saves energy and heat because that peak torque is generally required for a
22:04
small portion of the move usually the axle of the D so we typically see heat loads reduced up to 65 percent as a
22:11
result of that sort of automatic current adjustment now in addition to dynamically lowering the current draw
22:17
the step servers have the ability to peak the motor current up to 50 percent higher than the rated current of the
22:23
motor for short bursts very short bursts again taking that same example of the long move requiring the accel current
22:30
burst you can now potentially switch to a smaller motor since a three and a half amp motor can burst up over five amps
22:37
for a few seconds to get you through that high torque requirement or even better if you keep the same five amp
22:43
motor you can actually increase your available acceleration current to seven-and-a-half amps which enables faster acceleration
22:50
and with the fixed move length that means you can decrease your cycle time to increase your throughput with the
22:56
same size motor but now in this whole package you have increased cycle time and with the increased travel that the
23:02
integrated screw brings to the picture you really have a very efficient system switching gears to talk a little bit
23:09
about motor control you can see on that drive in the picture which is our SS M series there's a communication support
23:15
in this case of Ethernet and an i/o connector the drives have two basic operating modes standalone or streaming
23:22
control and we have a full suite of software configuration tools to help set up the drive as easily as possible
23:28
stand-alone drives can be programmed using our Q programming language to perform complex motion profiles react to
23:36
analog digital inputs and outputs and manipulate registers the programs can be executed automatically on powerup or
23:42
triggered by digital inputs and again all this is configured through our software tools streaming commanded
23:49
drives can be even more powerful when you have a plc or other control system in the mix in addition to being able to
23:55
support stored cue program execution the drives can be controlled and modern real-time over your preferred
24:01
communication protocol to monitor and command position IO States and Drive status one key advantage here is mixed
24:09
control mode operation for example on powerup you can program the drive to execute a complex homing procedure and
24:16
then set an output to tell your PLC that homing is complete and switch automatically in the step indirection
24:22
mode so wait PLC control and give the PLC confidence that the drive is now in an own home position so it can start
24:29
moving freely and then finally our drive support a lot of different field bus options for those plcs we have full
24:36
command and stored program execution over Ethernet IP EtherCAT can't open
24:41
Modbus TCP and rtu and we have a team of Apps engineers in California that can
24:47
support the various integration challenges from motor sizing and drive selections through field bus and TLC
24:52
integration issues all right let's run through a few different applications here we're going
High Accuracy Positioning
24:59
to talk about what the applications require and how the integrated leadscrew
25:04
motor can be a great fit for those applications first up is going to be a
25:09
high accuracy positioning type of application as you can see from the picture we've got a DLP printer that's
25:17
moving in a z-axis direction the key requirements for the application are a super-tight 20 micron layer resolution
25:25
we've got retract followed by a step move and of course if you see the word
25:31
printer in an application it's almost always going to be very cost competitive the way that the solution really shines
25:37
here is for the screw in that nut we offer the constant force anti backlash nut which is going to help with enhanced
25:44
repeatability the application is going to require bi-directional z-axis moves that's going to have a decent effect on
25:52
the column err viscosity so it should actually be benefit of using the type of
25:57
nuts that PBC offers and then we talked about the improved lead accuracy of plus
26:03
or minus three thousandths per foot so that could potentially eliminate the need for an encoder which of course if
26:10
you can start skipping out on encoders and then other components you're going to save money on the application the
26:16
smart rotor here this is going to use as I was mentioning before mixed control mode the home the hard stop feature
26:22
which is mentioned at the bottom there that allows you to have completely sensorless homing you can write a
26:29
program that's saved in the drive to monitor the position of the motor turn the current down very low and
26:35
essentially move the screw until your load hits a hard stop the motor can
26:42
detect that very quickly thanks to that encoder and you can back off and know ok now I'm in my home position and then you
26:49
switch over into seven Direction mode and the PLC can move knowing that you are in your home position
Digital Scanning
26:57
for the next one we've got a digital scanning application which is going to offer a nice horizontal move the key
27:03
requirements for the application are going to be minimum torque ripple and a precise lead accuracy again if we go
27:11
back to the complete PBC leads for motor solution to summarize we're offering a
27:17
superior lead accuracy for this application it's definitely required any variation in the lead accuracy results
27:24
in variable linear velocity even if the motor rpm is 100 percent constant anti
27:31
backlash nut is going to also help in this application be consistent preload
27:36
and the ability to maintain a consistent preload over the life is also going to be very important in regards to the
27:43
motor technology the whole system here is important not just one of the parts but all of them and with the addition of
27:49
0.9 degrees stepper the increased resolution on the full steps this kind of allows for better motion across the
27:56
entire plane allows for better resolution paired with the controls of microstepping just increases the ability
28:03
to scan in a consistent way across the length of the travel and then in terms
28:08
of the deep end torque everything that I've seen in terms of other motors that are out there available the deep end
28:14
torque is all over the place I've found that moons as motors have controlled the deep end torque to a minimum and quite
28:21
often our effect out much lower than competition and this also improves the
28:27
scanning capability without affecting the motion itself I'll let Mike talk about the controls a little bit again
28:33
this is using that same load torque ripple and 400 pull motor that you mentioned really with the 20,000 line
28:39
encoder we can achieve very very precise move profiles not much more to say than
28:44
that okay let's go over to the next application this is a high duty cycle application
High Duty Cycle
28:51
it's another printer this is actually going to look something like company that some of you might be familiar with
28:56
the three DP type of printer where it's a large scale large print type of application on this application we've
29:04
got high precision XYZ requirement of course we're 3d printing so we want to
29:10
add lair resolutions around 60 to 70 microns as you can imagine when you're printing
29:16
something you need a lot of short-stroke moves but then you also need to be able to move long distances up to one and a
29:24
half meters even at a fairly quick bead in this slide is saying 500 millimeters a second you've definitely got to have
29:31
reliable life on your product because a lot of these prints especially if you're
29:36
printing as it says here an engine block or I know 3d P is actually printed large
29:42
like scaled people the larger the print the longer it's going to take to printed and the whole time the print is taking
29:48
place the leadscrew motor everything else is moving continuously for that whole period of time and of course
29:55
anything that has the word printer in it it's got to be cost-competitive because everybody wants to get it done for the
30:01
least amount of money possible looking again at leadscrew motor solution we definitely want an anti backlash you nut
30:08
to enhance that repeatability we want to use bi-directional XY moves which again
30:13
the anti backlash nut is going to help with and then the lead screws that we offer have a variant lead availability
30:21
in this case the lead that was being used as a 25 millimeter lead we could accommodate all of those things with the
30:27
PBC offering in regards to the motors Jamie's mentioning the high lead and the
30:32
higher torque available from the motor in order to improve efficiency and throughput on the customer side because
30:39
when they're printing things they're not always necessarily printing but they need to translate from one position to
30:45
another and the quicker you can do that the more capacity you're able to get out of your print machine and process having
30:51
a motor that's got more torque allows you to do that with higher acceleration translate the move and then decelerate a
30:58
lot quicker so you've got that fine control in terms of miss steps etc all that might talk a little bit about that
31:04
because that's tied to the encoder and the controls one of the big advantages here again is that integrated encoder
31:11
when you think about a step in Direction application a lot of people think okay I'm going to feed a step in and the
31:16
motor is going to move one step with stepper motors without encoder feedback that's not necessarily the case the
31:21
motor is going to try to move one step but you have no idea whether or not it got there with these types of smart controllers on
31:27
the smart motor you can feed in steps and the motor is guaranteed to move that
31:33
number of steps long as your step input signal is cleaned the motor is going to make it there and it will let you know
31:39
if it's taking more torque it'll let you know if it's taking longer than expected but the motor will make it there let's
Application Solutions
31:46
look at an application solution for harsh environments and there's some gruesome pictures on the next slide that
31:51
look at some of the different types of motors that can withstand that for the screw material we haven't talked about
31:57
this yet at all the video talks about it a little bit of the screws are all 300 series stainless steel so inherently
32:03
those are going to be good for harsh environments we do also offer a PTF coating option which is why this screw
32:09
in the picture is black PTFE coating is going to reduce the wear it's going to
32:15
depend on the application again but around 20 to 30 percent reduce wear that's going to give you even more life
32:21
we do have specialty materials like I said it's a Delrin self lubricated with
32:27
PTFE we've also made custom brass and bronze nuts for customers depending on
32:33
the application and their needs and then of course the inevitable other options
32:38
if your customer has an application where they need something that doesn't look like we might have it let us know
32:44
and if the opportunities there for us then we will definitely be glad to look into that for you
32:50
this is an anti-corrosion technology that moons has available typically what customers do when they've got a harsh
32:56
environment is they try and seal all the electronics seal the motors and seal all the moving parts to avoid any sort of
33:03
ingress of external material whether it's liquid thus that kind of thing with humidity and liquid in particular
33:09
chances are with the temperature changes of the motor quite often the motor acts as a vacuum and inevitably some moisture
33:16
will get sucked in and if you're sealing the motor you're trying to stop the material from getting into the motor
33:22
itself which will cause it to die eventually but when you seal it you're actually stopping anything that does
33:28
come in from getting out as well there's two ways to handle that type of application what we do with the anti-corrosion is we do not seal the
33:35
motor itself but we coat all of these surfaces so we allow the moisture to come in and leave without affecting the
33:42
performance of the motor that's how we tackle out with this very unique product all of the materials are coated both
33:48
internal and external and the motor can run in extremely harsh environments and you can see what type of salt water does
33:54
to a standard motor on the left bottom picture versus to what the anti-corrosion motor looks like after
34:00
the same amount of time in the salt water spray test okay to summarize what
Summary
34:06
we talked about at the start was what a traditional the leadscrew motor looks like with the interface hardware and all
34:12
of the other motion controls and etc that are required to make that happen and then we compared that to the PBC
34:20
solution which is an integrated lead screw stepper motor it's also really worth mentioning one more time that this
34:26
can be ordered with one part number which in its own right is going to help save you time because you could go to
34:32
one place by one thing that accomplishes everything that the application is going to need it's going to increase your
34:38
performance with all the wonderful advances that Andy and Mike talked about and motor and control technology it's
34:46
also going to reduce your cost and it's going to reduce your size with that
34:51
being said I'm done Thank You Jamie Andy and Mike for a very
34:57
thorough presentation that was very well done if you do have questions you will
35:02
be able to reach the presenters and I'd like to thank you guys again for an
35:08
excellent presentation
Motion control for lead screw linear actuators is explored in this webinar. It covers the foundational elements of lead screw motors, including their design and integration, and highlights key applications such as automation, robotics, and precision machinery.