Case Study: Linear Actuators Drive 3D Printing for the US Marines

Linear Actuator Gantry System

Components:

UG Series Linear Actuators
300 Series WorkbenchPro 3D Printer

Retrofit or OEM:

OEM

Problem:

Linear actuators were essential for XFAB, which required a large format 3D printer equipped with a robust XYZ gantry system. The design had to ensure the printer could withstand various environments while delivering precise and reliable prototypes.

Solution:

Advanced linear actuators allowed the Marines to rapidly produce essential components and prototypes on-demand in diverse conditions.




Linear actuators from PBC Linear power the Marine Corps Tactical Systems Support Activity’s (MCTSSA) XFAB, a portable expeditionary fabrication lab for additive manufacturing, supporting maintenance, fabrication, prototypes, supply and equipment modification. MCTSSA, which aids the Marine Corps and Joint Service C4I architecture through communications exercises, cyber testing, and tactical networking, recently hosted design experts to test XFAB’s network connectivity. The lab features a 3D Platform 300 Series Workbench Pro large-format printer, enhanced by PBC Linear’s industrial-strength linear actuators. These actuators ensure superior performance and reliability, enabling precise, robust motion control for demanding field operations.

The Marine Corps and XFAB

XFAB is a transportable and self-contained, additive manufacturing lab that can be deployed with battalion-level Marine maintenance units. The lab is 20-by-20 feet and is collapsible for easier transport. Inside there are five 3D printers including two desktop printers, two industrial carbon fiber printers, and our 3D Platform 300 Series large format printer. In addition, the lab includes laser scanners and cutters, and a corresponding computer design software system.

The XFAB container is powered by a generator or shore power, and can be set up or torn down by a team of four Marines in roughly two-to-three hours. Its weight, when fully equipped, tops the scales at about 10,500 pounds and can be transported via the Logistics Vehicle System Replacement or a typical commercial flatbed truck.

XFAB has been in development for over five years, and will eventually provide Marines with an opportunity to fabricate their own manufacturing tools, parts, and signage. This unique capability will offer much-needed support in forward-deployed expeditionary environments where specialty and hard-to-find parts are not readily available.

3D printer gantry system with linear actuators

3D Platform 300 Series WorkbenchPro large format printer system

Linear Actuators SIMO Process

SIMO® and 3D Printers

The 300 Series large format printer from 3D Platform offers the highest print volume dimensions of the group, with a robust 1000 mm x 1000 mm x 700 mm (0.7 m³, 1.4×). It is built with linear motion hardware that includes SIMO Series actuators from PBC Linear. Each actuator that moves along the X-Y-Z gantry is customized and incorporates Constant Force™ anti-backlash lead screws and nuts for simultaneous high precision and strength.

SIMO is an acronym for Simultaneous Integral Milling Operation. It is a process developed and patented by PBC Linear that has revolutionized traditional machining. The SIMO process uses synchronized cutters, eliminating built-in extrusion variances by machining all critical edges concurrently in one pass. This ensures tight tolerances, limited variance, and a remarkably straight and repeatable surface at minimal additional cost. This process is used on both our plain bearing Gliding Surface Technology and related actuators, as well as cam roller V-guide bearings.

The SIMO process offers many advantages to the standard aluminum extrusion process. The twist and flatness are generally two times better than standard aluminum extrusions, with the straightness (camber) reaching six-times that of standard extrusions.

Demo Day

The testing event at MCTSSA included senior leaders and Marines from 1st Marine Logistics Group, 1st Light Armored Reconnaissance Regiment, 3rd Amphibious Assault Battalion and 3rd Marine Aircraft Wing. The demo offered them a first-hand look at the equipment and how they can manufacture parts and products. The main goal of this event was to first evaluate the connectivity of the Marine Corps’ closed computer network and then determine if any adjustments are needed. The ultimate objective is to reach final operational capability and then begin delivering labs to the Fleet Marine Forces by June 2022.

Discover the best linear actuator solution for your application:

3D Printed Part

U.S. Marine Cpl. Tyler Anglin from 1st Maintenance Battalion holds a 3D printed universal load stud wrench during a demonstration event at Marine Corps Tactical Systems Support Activity. This and the top photo by Amy Forsythe / U.S. Marine Corps.

‹ ›
Cite This Page

Source: PBC Linear - “Case Study: Linear Actuators Drive US Marine 3D Printing Solutions”
https://pbclinear.com/blogs/application-stories/simo-series-and-3d-printer-supports-marine-corps
Last updated: November 2025