Components:
Retrofit or OEM:
Problem:
Solution:
The challenge of developing a good Idea
The first working prototype was presented to DT Engineering, a specialty engineering firm that focuses on machine design, build, and replication (build to print) of custom machinery. Their task was to bring in a more refined design that increased manufacturability, decreased machine complexity, and operated reliably. One issue with the original design was the numerous linear motion components that made up the system. Rails, mounting parts and fasteners, and pillow blocks combined to take up a considerable amount of space resulting in a complex assembly. They used a modular approach for the internal sub-assemblies and sought out maintenance-free components for longer-lasting performance.
The PBC Linear solution
DT Engineering began by working closely with PBC Linear to simplify the linear motion system, and finally decided on their Uni-Guide linear slide for the three critical tasks of the book printer. The simple, two-piece rail and carriage assembly of Uni-Guide provided a more streamlined design without bulky mounting pieces or painstaking assembly work. In addition, the carriage's internal Simplicity® plain linear bearings glide smoothly and reliably without the need for additional lubrication or preventative maintenance. The rails have dual shafts that are precision machined along the edge to ensure perfect alignment and parallelism. All of these Uni-Guide advantages were essential to improving the performance of the Espresso machine’s smooth cutting of the book pages, gluing of the pages to the cover and spine, and collating the pages for binding. All in all, the Uni-guide provided long-lasting transfer and adjustment for some of the Espresso’s most important operating tasks.
Results / ROI
By implementing Uni-Guide technology from PBC Linear, DT Engineering was able to reduce each linear motion assembly from roughly 10 pieces down to 2, creating a simpler, cost-effective printing machine. Today, the on-demand Espresso Book Machine is now available in college libraries and bookstores worldwide. It can automatically print, bind and trim a perfect bound, bookstore quality paperback at the point of sale, eliminating the need for overstocked inventory. The Espresso also boasts the added value of offering rare, hard to find titles. Books are first selected using EspressNet® software developed by On Demand, and then printed within 2-3 minutes. The final book is complete with front/back covers and is ready for immediate sale.
Discover the best linear guide solution for your application:
- Find more information on Uni-Guide Linear Slide Guides
- Request your FREE product sample
- Request a quote
- Contact an engineer