Case Study: Linear Actuator Monitors Paper Production Line

Linear Actuator used as a Monitoring Device

Linear actuators can measure moisture content

Variances in paper production can lead to degrees of moisture being present in finished paper. While a clean sheet of everyday paper is dry, it actually starts out as a liquid pulp that is pressed into the dry sheets used for writing, drawing and packaging; therefore, measuring moisture content in paper is an effective way to ensure quality of product. Paper production can consist of many different thicknesses and weights; which makes it difficult to manually determine if there is moisture present as the product is moved down the production line.

Retrofit or OEM:

OEM

Problem:

Monitoring the moisture content in paper production requires precision motion control.

Solution:

An MTB linear actuator from PBC Linear provided smooth, oscillating travel perfect for the application.


MTB Linear Actuator to the Rescue

A linear actuator, specifically the MTB042 from PBC Linear, was installed over the production line at the paper manufacturer. The MTB’s carriage was equipped with a moisture sensor to measure moisture levels in the paper passing underneath. Featuring a steel-reinforced timing belt, the MTB provided smooth, oscillating travel for the required 100" stroke. This configuration allowed the sensor to accurately measure moisture content without interrupting the paper production process.

 

Discover the best linear actuator solution for your application

‹ ›
Cite This Page

Source: PBC Linear - “Case Study: Linear Actuator Monitors Moisture in Paper Production Line”
https://pbclinear.com/blogs/application-stories/measuring-moisture-in-paper
Last updated: November 2025