Adjusting Belt Tension on Linear Actuators

Adjusting Belt Tension on Linear Actuators

Belt tension is set at installation on the belt driven linear actuators and regular maintenance then becomes a big key to keeping them at top performance. It is a good practice to periodically check the belt tension and make sure that it is set properly. Follow these simple steps to adjust belt tension on the MTB series linear actuators.


  • Remove and disconnect the drive mechanism from the actuator.
  • Move the carriage to the point specified in the actuator’s written maintenance instructions. This point will vary depending on the model and size.
  • Remove the cover plate over the belt tension adjustment screw at the idler end of the actuator.
  • Remove the seal strip clamp from the idler end of the actuator.
  • DO NOT CREASE the SEAL STRIP, but slide it back out of the way.
  • Using a force gauge, determine the amount of existing deflection in the belt. Refer to the written instructions for the amount of deflection required for the specific model and size.
  • Locate and loosen the set screw on the clamp collar. This will then allow movement of the belt tension adjustment screw.
  • Adjust the belt tension adjustment screw to obtain the proper belt tension.
  • Measure again with the force gauge to ensure that belt deflection is properly set.
  • Tighten the set screw on the clamp collar to lock the adjustment screw into place.
  • Use a medium-strength thread locker on all fasteners for steps 12 – 14.
  • Re-install the belt tension adjustment screw cover plate.
  • Slide the seal strip back into place.
  • Re-install the seal strip clamp.
  • Reconnect drive mechanism to the actuator.
›
Cite This Page

Source: PBC Linear - “Adjusting Belt Tension on Linear Actuators”
https://pbclinear.com/blogs/blog/adjusting-belt-tension-on-mt-actuators
Last updated: October 2025