Case Study: Plain Linear Bearings for Rug and Carpet Tufting Equipment

Plain Linear Bearings in Carpet Tufting Application Story

Carpet manufacturer turn 95% of scrap losses into gains

Carpet tufting creates a tough environment for linear motion products. In this process, synthetic fibers are applied to a carpet backing using a high-speed machining system. The needle bar, which holds 4,000 tufting needles, employs quick and reciprocating short strokes up to 1600 cycles per minute. The carpet tufting machine is designed to run for long, continuous stretches, and therefore the performance is measured by the life of the system, along with the amount of linear feet that are run between replacement systems.

Retrofit or OEM:

Retrofit

Problem:

High speed reciprocating short strokes create high impact loads on the system, resulting in worn ball bushings and shafting. 

Solution:

Simplicity plain linear bearings contain no rolling elements, thrive in heavy load applications, and push contaminants such as dirt, carpet fiber particulate and grease to the end of the stroke.


Tufting tale

In this scenario, each carpet tufting machine used 36 linear ball bushing bearings and steel shafting assembled into a push-down foot system (4 bearings and 2 rods of steel shafting per push-down foot, for an average of 9 push-down feet per machine). Precise and repeatable linear motion would be essential for optimum manufacturing and the minimization of scrap. The manufacturer also employed non-stain oil along the pushdown foot assembly to ensure smooth linear motion and reduced friction.

The environment of the application is typical for industrial machining. While no adverse or caustic chemicals were present, contaminates such as dust, dirt, grease and carpet fiber particles posed a substantial risk for contamination.

Carpet Tufting Figure 1

The Losses

This carpet manufacturer was experiencing unplanned downtime due to linear bearing failures and massive profit loss due to thousands of yards in scrapped end-product. Poor quality and damaged carpeting were cited as the main reasons the manufacturer lost up to 54,000 yards of carpet to scrap. The root of the problem was found to be the machine’s ball bushings within the push down foot assembly. Specific issues included:

  • High-speed reciprocating short strokes (.5"-.625") that created high impact loads on the system, resulting in high wear on the ball bushings and shafting. This was the main cause of shutdown scenarios where maintenance and product replacement were necessary.
  • High cycle/minute stroke rate that raised high reverse inertia, prompting almost immediate wear of the ball bushings and steel shafting.
  • Spalling from the ball bushings against the shafting created fine metal particulates that accumulated within the assembly, wearing out the seals, and eventually allowing lubricants to contaminate the pushdown foot assembly and ball bushings. These lubricants then mixed with metal particulates to create “black spots” on the finished carpeting. The black spots could not be washed out, resulting in more scrap carpet.
  • Inaccurate tolerances (.005/.007’’) of the ball bushing system which caused a rocking motion along the needle bar. This phenomenon, known as needle wander/loss motion, caused inaccurate positioning and missed tufts, leading to poor quality carpeting. This occurred almost immediately after the initial installation and grew more prevalent as the system wore down. Throughout the operation, loss motion and contaminated carpet resulted in 34,000-54,000 yards of scrap material and lost profit.
Carpet Tufting Figure 2

The PBC Linear Solution

PBC Linear implemented their Simplicity® self-lubricating plain linear bearing into the pushdown foot assembly for the carpet tufting machine. Its close tolerance ID bearing (.6240”-.6245”) and close running clearance (.0015”-.0018”) held the needle bar in tight position. This solved the problem of wear and progressive wander/loss motion.

The bearing’s proprietary FrelonGold® liner ran smoothly along the steel shafting, eliminating wear by evenly disbursing the load throughout the bearing. This successful solution was noticeably different than the previous application, which had only a small point of contact between the ball bushing and shafting products. Since Simplicity bearings contain no rolling elements and thrive in heavy load applications and dirty environments, they were able to push contaminants such as dirt, carpet fiber particulates, and grease to the end of the stroke.

The Gains

Simplicity linear bearings were designed to exceed expectations in applications like this. Before Simplicity bearings were installed in the pushdown foot system and undercarriage, the carpet tufting machines were in a state of constant unplanned downtime due to high maintenance costs and upkeep. Now, these updated carpet tufting systems have become the most productive machines in the plant! The linear footage between maintenance rebuilds of the machine were increased from one million linear feet to over three million. The carpet manufacturer was also pleased to report a significant 95% reduction in scrapped product, eliminating millions of dollars in scrap every year that was previously thought of as “an acceptable loss.” Those losses are now profit gains!

Discover the best bearing solution for your application:

‹ ›
Cite This Page

Source: PBC Linear - “Case Study: Plain Linear Bearings in Carpet Tufting Machinery”
https://pbclinear.com/blogs/application-stories/carpet-tufting-is-a-tough-environment
Last updated: November 2025