LSG (Inch) Linear Steel Low Support Rail and Shaft Set


Precision case hardened and ground shaft, plus a steel low support rail, effectively doubles the life of the shaft by allowing it to be turned over for a fresh surface when wear becomes evident. Both sides of the shaft are counterbored so the shaft may be rotated 180°, and rebolted for use on the new side. This guide is sold as a two-piece set; the shaft and support are not assembled. The guide is then bolted down through the top of the shaft to reduce installation time. The shafts are also available in 440C stainless steel. Drilled through and counterbored shafts may not be suitable for all linear bearings.
No coating